Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Product List
POWR1014A-Slide7

The Hercules Development kit demonstrates the POWR1220AT8. It has been added to support the POWR1014/1014A products because it offers a complete demonstration of functions that the POWR1014A breakout board does not. The board is preprogrammed allowing evaluation of various functions. A slide switch demonstrates a voltage rail varying in and out of regulation. LEDs give visual verification of sequencing, power good, variable watchdog timing and reset. A push button allows a change of mode that is selectable by setting demo dip switches. An additional CPLD and FPGA have been added to allow reading of voltages and display on the LCD display. The device can be reprogrammed to test other functions through the JTAG interface or through the USB port. Voltage measurements can be reported through the USB port.

PTM פורסם ב: