Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Product List
IPN De-Rating with Temperature

The GO is the first current sensor IC to withstand 30 A RMS continuous at 105°C. The limiting factor is the thermal dissipation of the primary conductor jumper within the device. With 1.1 mOhm resistance, the dissipation is minimized.

PTM פורסם ב: