Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Product List
BusBuffer-Slide2

I²C is a popular digital interface used for short-range chip-to-chip communication. It features a simple 2-wire bus, ease of implementation, and up to 400kHz operation in fast mode. As with any other standard, designers may run into issues when their application pushes the original I²C specification to its limit or when the specification falls short in addressing today’s requirements. As systems become more complex, more I²C devices are added to the bus and may start to compromise certain parameters. This slide shows some of the most common issues that I²C system designers face today. They will be addressed throughout the rest of this presentation. The varieties of issues are of electrical, timing, or signaling nature.

PTM פורסם ב: