Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Product List
LTM8047-Slide5

A table summary of the electrical features comparing the LTM8047 and LTM8048 is presented with the key differences highlighted in yellow. Again, the LTM8048 has an internal post-regulation LDO, reducing the output ripple to 1mV peak to peak in comparison to the LTM8047 at 35mV peak to peak. These two isolated converters are the latest addition to the innovative µModule® power products family which includes battery chargers, LED drivers, step-down, and step up and down regulators.

PTM פורסם ב: