Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List
Encoder-Slide12

This chart shows a simple comparison between the different Linx encoder and decoder products. The MT Series offers bi-directional remote control with confirmation. This should be selected for applications where the 2-way communication is needed. The MS Series is legacy and is being replaced by the MS2 Series. The MS2 offers the encoder and decoder in one part for a lower cost with the same functionality. It has a large 24-bit address and a smaller hardware footprint than the DS Series. This should be selected for applications where a greater degree of uniqueness is necessary or where the single button push addressing is desired. The HS Series offers a high degree of security with an encrypted link. This should be selected for applications that need the security. The DS Series should be selected as a replacement for Holtek products or because of the simplicity of its DIP switch addressing.

PTM פורסם ב: