Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Product List
Image of Littelfuse High-Speed Fuseology - Selection Parameters Summary

This slide will briefly review the key parameters for fuse selection that will help narrow down potential fuse options for a specific application. There are five key selection parameters that should be used to help identify potential fuse solutions. These parameters include: voltage rating, amperage rating, interrupt rating, total clearing I2t, and peak arc voltage. These high-level parameters help filter out many of the fuse options that exist in the market. Once a fuse meeting these key parameters is identified, a more detailed application design can begin.

PTM פורסם ב: