Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Product List
The Problem

This study was conducted in the US by the National Electoral Manufacturers Association (NEMA), and the statistics are similar internationally. When people think of surge protection, the first thing that comes to mind is lightning protection. However, based on the study, 60 to 80% of surges come from within a facility, and lightning only accounts for about 22% of surges.

PTM פורסם ב: