Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Product List
Flexible-Slide3

There are two primary types of backlight technology: edge lit and chips on board. In both types of technology, LEDs are used as the light source that focuses light into the light guide which then distributes the light evenly behind the viewing area. As its name implies, an edge lit backlight is constructed of LEDs that run along the outer axis of the backlight.

PTM פורסם ב: