Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List
reading teg
Because multiple curves are provided on the datasheet of the thermoelectric generator, the proper curve needs to be selected. Select the curve with the cold side value TC representative of the application. Then, draw a vertical line on the graph through the hot side temperature axis that corresponds to the application hot side temperature. Optimal power output can be determined by drawing a horizontal line from the intersection of the power curve and the hot side vertical line drawn in step 2 to the Power axis. Optimal voltage output can be determined by drawing a horizontal line from the intersection of the voltage curve and the hot side vertical line drawn in step 2 to the Voltage axis. The intersection of the vertical line from step 2 and the bottom indicates the heat transfer rate through the TEG module for the given operating condition.
PTM פורסם ב: