Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Product List
MAX11300 Programmable Mixed Signal IO Pt 2 Slide 5
Once the designer is satisfied with the configuration, a .CSV file is generated with the registers addresses and corresponding register values - this becomes the programming bitstream to be downloaded to MAX11300 through the SPI interface. This .CSV file may be read with a GUI for downloading to target hardware, for example Munich GUI and MAX11300PMB1, or embedded within code for programming a PIXI device in the end application.
PTM פורסם ב: