Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Product List
MAX31865 RTD-to-Digital Converter Slide 10
To protect against overvoltage faults of the RTD, each of the five inputs of the MAX31865 features a high voltage MOSFET analog switch that opens if the voltage at the input of the switch is greater than VDD or less than ground. The design protects against overvoltages in the ±50 V range.
PTM פורסם ב: