Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Product List
grid-EYE
The Grid-EYE is a small, surface mount sensor in a ceramic package. The 8x8 array can provide separate temperatures for each pixel and with a high gain version, an engineer can achieve an accuracy of ±2.5°C for the outer pixels with the ability to get an even more accurate reading using the center pixels. Detection speeds of one frame per second or ten frames per second can be selected based on use case with the option of slowing down even further for energy saving.
PTM פורסם ב: