Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Product List
MCU-Slide15

This example shows an OpAmp being used for basic signal conditioning. The DAC is referenced to the internal FVR, an adjustable offset voltage is then fed into the OpAmp, a simple resistor network is used to set up the gain of the signal. The result is granularity exceeding 12-bit, with a 10-bit ADC, for the critical portion of the signal being measured.

PTM פורסם ב: