Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Product List
PIC24F Curiosity Development Board Slide 6

For the user’s convenience, an “out-of-the-box” demo is pre-loaded into the PIC24F Development Board system. In this demo, a red-green-blue color mixing application, the potentiometer can be used to adjust each color channel intensity, independently, while the push buttons are used to select the channel to be adjusted. The programmer/debugger on board requires MPLAB X Cloud-based IDE version 3.4 or later on the development system. In addition, there are also a few Curiosity board MikroElektronika Click board demo’s available. Details and links can be found on a slide near the end of this presentation.

PTM פורסם ב: