Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Product List
ek1 Linux4SAM homepage
Microchip provides a complete development system for the SoM in the ATSAMA5D27-SOM1-EK1. The board provides connections for a TFT-LCD screen, camera interface, Ethernet, USB, SDIO interface including a microSD slot and two sockets for Mikroelectronika Click boards so designers can begin product development using this board. Full software board support packages can be found at www.linux4sam.com.
PTM פורסם ב: