Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Product List
OFP-Slide7

The Mill-Max 834/835 series Pass-Through Sockets are an assembly of loose pin receptacles into single and dual-row insulators. These sockets are an ideal way to mount numerous receptacles at once. This series has a low .130” profile and will accept .030” diameter round pins, as well as industry standard .025” square pin headers. As with loose receptacles, the OFP® Pass Through Sockets are designed for hand, wave and reflow solder processes. The unique advantages these sockets offer is the ability to connect more than two p.c. boards together, and component leads of any length can be accommodated.

PTM פורסם ב: