Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Product List
Heavy Duty Rectangular Connectors Slide 5

The Second components is the Hood. The Hood enclosure connection would typically be at the end of a cable and would be used with a Cable Gland. The Hood will normally have two or four pegs to accept the latching system of its Housing enclosure counterpart. The Hood image shown here on the left is an example of a single latching, side cable entry system with 2 pegs. The Hood image shown on the right is an example of a reverse double latching, top cable entry system. The Molex GWconnect line of Heavy-Duty Rectangular Hoods are compatible with various competitor inserts for easy replacement.

PTM פורסם ב: