Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Product List
Full Duplex Data Throughput

The performance, or throughput, of a Peraso accelerator engine device can be tuned by selection of the SerDes frequency, the number of SerDes lanes utilized, and the selected burst size. The vertical axis shows the effect of number of lanes used and burst length, while the horizontal axis reflects the SerDes rate used. The value pictured in the boxes is the value of the data throughput. So in the case of a 16-lane, burst of 8 to 25 Gbps device, the value is 320; this reflects the fact that 320 Gbps of data is transferred. This has already taken out the overhead of the protocol, so this is pure data throughput. Also, realize that this reflects 320 Gbps at the ingress of the device as well as 320 Gbps at the egress of the device, which results in 640 total throughput of the device. In relation, the blue, red, and green lines reflect the equivalent throughput of the RLDRAM, QDR IV, and Sigma Quad devices on the market.

PTM פורסם ב: