Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Product List
Accelerator-Slide12

Each communication frame contains 16-bits. The first 8 bits in the MOSI line contains info about the operation (read or write) and the register address being accessed. The first 6-bits define a 6-bit address for selected operation, Bit 7 defines which operation is performed (write or read). The 8th bit is an odd parity bit for 8-bit pattern. The later 8-bits in the MOSI line contain data for a write operation and are ignored in case of read operation.

PTM פורסם ב: