Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Product List
Ferrite-Slide17

Automotive ferrite beads are also available from muRata. Automotive ferrite beads comply with AEC-Q200 requirement, to meet the stringent needs of the automotive market. As users can see in the illustration on this slide, there are several Automotive applications that require some form of EMI noise suppression. These applications include Back-up Camera, GPS, Navigation, RKE, Radio, and Infotainment.

PTM פורסם ב: