Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Product List
NHDev LCD Development Board Slide 5

After successfully connecting the display to the NHDev LCD Development Board, adjust the jumpers on the board to the required power supply, 3.3V or 5V. Then, select either VDD or VEE according to the display’s specification (also found on the wiring diagram). Next, select the backlight supply voltage and move the jumper accordingly. The NHDev LCD Development Board is now ready to have power applied.

PTM פורסם ב: