Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Product List
A/D Converter Applications

When using an analog switch in A-to-D converter applications, remember to consider the following in the design: the input signal voltage range, the ON resistance, the signal bandwidth required, the impact of the input RC filter that will impact the sample time, the isolation between the input channels, and the allowable total harmonic distortion (THD).

PTM פורסם ב: