Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
Image of Nexperia LFPAK88 MOSFETs - Easy Paralleling

With the power levels increasing in a number of different applications within the car, the paralleling of MOSFETs is becoming more common. When paralleling the MOSFETs the designer wants them to turn on at the same time; otherwise it could lead to current imbalance in the circuit which will lead to problems. One way to ensure this is to have a tight threshold voltage spread. The 40V superjunction products have a threshold voltage spread of 1.2V.

PTM פורסם ב: