Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Product List
FPCAP-Slide21

In summary, the FPCAP family of capacitors from Nichicon are constructed with conductive polymer aluminum material, which provides a smaller overall case sizes and lower ESR than standard aluminum electrolytic capacitors. Nichicon also offers a wide selection of radial-leaded capacitors in the FPCAP family with the NS, R7, R5, NU, L8, S8, E5, HT, F8, NE and in surface-mount the PS, PA, FS, SS, SA, SB, HS, HA, SL, SH series.

PTM פורסם ב: