Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Product List
RF-Slide4

The movement of air through a system is accomplished by the creation of a pressure drop across that system. The airflow generated by a fan at a specific pressure is directly related to the cooling it can provide. NMB’s R and F Series fans deliver some of the highest flow rates available today, for both Axial and Radial fans in the 172mm to 280mm size range.

PTM פורסם ב: