Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Product List
Thermal Simulation in Telecom Applications Slide 2

The fan, like the heart, helps regulate internal temperature, which is fundamental to the preservation of both a body and a computer.  If the internal temperature of a computer rises too high, crucial components will fail to operate properly. In fact, the fan can be thought of as the heart of any system: if the fan fails, other critical components are at risk of failure, thus leaving the entire system compromised and likely inoperable.

PTM פורסם ב: