Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Product List
depending on proc
The processor state, which can be either ARM or Thumb, and the processor mode determine which registers are available to the programmer. The processor mode determines which one of several register banks is accessible. In Thumb state, the register set is a subset of the ARM state register set.
PTM פורסם ב: