Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Product List
isp link lpc tools page
In-System Programming, another Flash programming technique can be accomplished with the LPC2000 Flash Utility. This utility causes the Flash to be reprogrammed via UART0 without the device being removed from the application board. The Flash on-chip Boot Loader provides the interface for the In-System Programming.
PTM פורסם ב: