Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Product List
Inst Arch

This presentation will begin with an understanding of the Cortex-M0 instruction set. The Cortex-M0 is a RISC or Reduced Instruction Set Computer architecture based on the ARM thumb concept. The complete instruction set for the Cortex-M0 can be seen in this diagram. Almost all of the Cortex-M0 instructions are 16-bits in length but operate on 32-bit registers and 32-bit data paths. The only 32-bit instruction used in application code is the B-L or Branch with Link instruction.

PTM פורסם ב: