Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Product List
coldfire-embedded-slide7

Once it is compressed, the packets can be sent out over the network. The connection over the network is controlled by the core control and signaling module popularly referred to as the SIP stack, although the SIP stack itself is only one component of this block. After that is a standard interface to the network with the TCP/IP protocol going out over the Ethernet network. 

PTM פורסם ב: