Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List
RT1050-Slide8

This slide shows how the i.MX RT1050 leads its main competitors with the comparable part numbers, by a factor of 2 to 4, both in CoreMark and power consumption in active mode. The i.MX RT1050 has an active current of 110µA/MHz @ 3.3V which is at least half of the nearest competitor.

PTM פורסם ב: