Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Product List
Support 2

Finally, NXP is expanding its LPC1700 series beyond the LPC1760 and LPC1750 series. The LPC1770 and 80 series add new peripherals and functionality while maintaining the lead in performance over the competition. These new series are pin-compatible with the popular LPC2400 ARM7 series from NXP. The LPC1770 and 80 series start with the LPC1760 and adds additional RAM, an external memory controller, an SD Card interface, 4 K-bytes of EEPROM and larger packages. The LPC1780 series is also the first Cortex-M3 microcontroller with an LCD panel controller. 

PTM פורסם ב: