Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Product List
1 mag
The space savings are even greater for high pin count devices, such as for a 56 pin device. A leadless replacement to an SOT371 can bring up to 82% of PCB space savings by utilizing a modified pin-out. The SOT1033 shown here uses a double row of pins along all four sides of the package, as opposed to a single row of pins on just two sides of the package. This simple technique drastically reduces the package footprint.
PTM פורסם ב: