Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Product List
Save Power

The LPC54100 contains another feature that can save power if the application does not use all of 104 KB of RAM. The SRAM is divided into multiple blocks and each block has a separate power switch. With this feature, a developer can selectively turn on or off one or more RAM blocks to optimize power consumption. Note that the first three blocks are contiguous while the four block is not.

PTM פורסם ב: