Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Product List
G3RI/O: Compact SSR for Interface with High Dielectric Strength Requirements

The G3R relay series carries forward the same logic as the G3RV-ST relay in that it is the solid-state version of the G2R relay series. This is a high-speed switching SSR with a high dielectric strength of 4 kV when used with a coupler.

PTM פורסם ב: