Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Product List
super small
The S-VSON family is small. The small size allows for high density mounting while providing size reduction in the customer’s end product. Also, it has a high switching capacity that previously was only achieved with bigger sized relays. Low C x R Models help to preserve the integrity of the signal. The dielectric strength is more than double the competitor’s models, making the G3VM S-VSON vastly more robust to transients. Suitable for using in testers that evaluate under high temperature, such as Automotive Testers and a smaller energy loss due to the low on-resistance.
PTM פורסם ב: