Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Product List
Flash Overview and Applications Slide 13

In summary, onsemi Flash memory is made up of arrays of floating gate transistors. There are three types of Flash memory: NOR Serial Flash, NOR Parallel Flash, and NAND Flash. Flash memory is non-volatile, offering a read access time as fast as dynamic RAM. Flash memory has a very fast program time but a slower erase time compared to EEPROM. Careful consideration must be used to select the correct Flash memory depending on the application. onsemi offers a broad portfolio to serve a variety of applications.

PTM פורסם ב: