Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Product List
spac sav
Shown here are the advantages of the power terminals with regards to current through-put. Each signal pin is capable of carrying 0.3 A current. This means that in a traditional type connector, in order to get 1.5 A of current, one would be required to connect 10 signal pins together in parallel. Now, with Panasonic’s power terminal connector, the engineer can deliver 3.0 A of current through each end allowing the pins in the center to be dedicated to transferring signals. This will allow for customers to reduce the overall pin count and save space on the board.
PTM פורסם ב: