Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Product List
This slide shows the installation procedure for the Graphite-PAD. Flat tweezers are recommended to first separate the top release film from the material and, second, to remove a part of the Graphite-PAD from the bottom release film. Care should be taken when handling/releasing the material due to its softness and compressibility. Once about one third of the pad is released from the bottom release film, the remaining portion may be removed by hand and then placed back on the release film until installation.
PTM פורסם ב: