Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Product List
Ethernet-Slide6

Once the customer has decided to go down the copper path, shown here are some of the benefits. One thing to keep in mind when using copper is that there are two types: solid and stranded. When using a stranded copper cable, which is typically used going to the edge and for more flexible routing, the cable needs to be derated.

PTM פורסם ב: