Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Product List
FiberOptic-Slide11

The OptiCam II termination and test tool is unique to the market. It is very easy to terminate fiber and then validate that the connection made was a good one. It uses a non-visible laser and internal ‘camera’ to provide a calculated insertion loss at the point of termination. It is then able to sync via Bluetooth® to a tool for termination data or to export to a CSV file for analytics.

PTM פורסם ב: