Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Product List Associated Content
Ink Jet Label Printing

Ink Jet printing is also a well known type of print technology that has grown beyond the original applications of office or home users. Ink Jet printing is great for lower cost printing in full color. These printers are easy to use and ink jet cartridges are easy to replace or refill. Liquid ink is used to create the printed characters. The most popular attribute of Ink Jet printing is the ability to print in full color with very high resolution up to photo quality and beyond for printing of industrial and commercial graphics. The one down side to Ink Jet printing is it is not as good as Laser Jet print durability. Thus, Ink Jet labels are not as commonly used for applications where extreme environmental exposure is a concern. Ink Jet printing durability is improving though with each new generation of printers, ink cartridges, and label materials.

PTM פורסם ב: