Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Product List
TIAMICE-Slide12

The typical style of cabling solutions in the industrial space are stranded, shielded, have a TPE or PUR jacket and are Cat 5E or 6. As the environment gets harsher, there are M3I3C3E3 style of cables, but for the general purpose industrial cable, the designer can use a cable with a harsher jacket style and shielding. If there are high voltage devices that are around the area that the cable is being pulled, there is 600V rated cable available. The nice thing about this cable is that it’s also high flex, which allows it to be placed on devices that are moving. For the harshest types of environments, such as oil and gas, there are special types of cables, such as those that are mud resistant. For these type of applications, it is best to talk to a technical resource to have them help identify the best cable types.

PTM פורסם ב: