Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Product List Associated Content
Dielectric Properties - Dry

Dielectric Properties refers to the voltage breakdown rating of the dielectric pad, typically tested per ASTM D149 and measured in kVAC. This is an average of 5 tests of the materials resistance to having voltage penetrate through the pad. It is therefore possible to have 1 or more results well below the voltage breakdown rating specification and yet still have the average of the 5 tests material that passes the specification limit. This table here is based on voltage breakdown of material at normal humidity conditions, typically 40% to 50% relative humidity.

PTM פורסם ב: