Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
PCB Retainer Overview Slide 9
When the retainer is engaged the wedges expand, clamping the PCB to the cold wall. The thermal transfer depends on several factors. Generally speaking for Wedge Loks, the larger the profile, and the more segments, the greater the heat transfer. Specialty metals can be used for additional thermal performance. In order to yield optimal clamping force, thermal Wedge Loks must be installed properly, using a calibrated torque wrench, to the specified amount of torque for that particular model.
PTM פורסם ב: