Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Product List
DIN Rail Terminal Blocks Slide 5

Spring-cage terminal blocks were developed for universal spring-loaded conductor contacts. The contact force is independent of the user, so that creates a vibration-proof, gas tight connection with long-term stability. The terminal point is opened with a standard screwdriver. After the wire conductor is inserted into the clamping cavity, the screwdriver is removed and the conductor automatically makes contact. This easy operation is performed as a result of front connection, where the conductor and screwdriver enter in parallel from the same direction. A variety of copper wires can be clamped without pretreatment. Use of ferrules prevents unwanted splicing. The spring element of the spring-cage is made from high-strength chromium-nickel spring steel.

PTM פורסם ב: