Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Product List
Features3

The THERMOMARK GO.K can store up to twenty created files in its system. Along with the full keypad, there are also over two hundred symbols that can be used when creating labels. It has barcode and sequence capabilities, and templates can be created for both flag and cable labels, as well as for terminal block spacing. While the user has the ability to create files directly on the device, files can also be created using the PROJECT complete marking software on a PC.

PTM פורסם ב: