Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Product List
USB 3 Overview Slide 8

The definition of a Half-Duplex system is one that provides communication in two directions, but information can only be transmitted in one direction at a time. A good example of this type of system are two way radios, “walkie-talkies”, when one handset is transmitting the other handset cannot transmit back until the initiator has completed its transaction.

PTM פורסם ב: