Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Product List
Creepage and Clearance

Creepage and clearance are also an important aspect for medical applications. Creepage is defined as the shortest distance between two points measured by following the surface between the points. Clearance is the shortest distance between two points measured through the air. RECOM medical-grade converters are fully potted. The creepage and clearance distances for these are measured between the external pins because the potting compound acts as an insulator.

PTM פורסם ב:
PTM Updated on: 2020-05-04