Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Product List Associated Content
Image of Renesas CK-RA6M5/CK-RX65N Cat-M1 Cloud Kits with RYZ014A PMOD - End to End Solutions

The crux of best user experience is to provide a complete solution which includes MCUs, sensors, and connectivity options for cloud connectivity. The cloud kits CK-RA6M5 and CK-RX65N are Renesas’ first complete cloud solutions which include Renesas MCUs, Renesas sensors, and Renesas CAT-M1 module. The key benefits of cellular are: It is easy-to-add on as it does not require any other equipment to connect in order to access internet at the site and secure connectivity. The closed cellular network provides an easy and secure communication path. In addition to CAT-M1 connectivity, the kits also include an Ethernet PHY, also a Renesas part to ensure a single source of key components and ensured interoperability. More wireless connectivity options will be released to ensure a consistent user experience regardless of the connectivity choice.

PTM פורסם ב: